Return Fan (MASD) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

This option adds a BO for the Return Fan start stop. Return fans can be constant speed or variable speed fans. Constant speed fans do not have additional options. The Variable speed fan option is only available if the Supply Fan is configured as Variable Speed.