Economizer Damper(s) (MASD) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

These selections provide the logic for the Economizer Dampers. If no economizer control (Free Cooling) is required, these options should not be selected (use Two Position Min OA Damper instead).