Coils (Preheat) (MASD) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

These selections provide the logic to control a Preheat coil. A Preheat coil may be located in the Outdoor Air Duct (ahead of the mixing plenum). If this is the case, a Preheat coil is always set to Control to Preheat Air Temperature. When in the Mixed Air Duct, the coil may either be controlled by a dedicated sensor or sequenced with the other devices. During startup, if a DA-T or PH-T sensor is available, the Preheat coil is controlled by the LT-SP (Low Limit Setpoint).