Shutdown AHU When Pump is in Alarm (MASD) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

For applications with Preheat pumps, the Shutdown AHU when pump is in Alarm option prevents the unit from starting if there is a fault in the preheat pump during cold weather.