Proportional Actuator (MASD) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

Proportional Actuator can be selected if the coil is controlled by a proportional valve that takes a 0–10 VDC or 4–20 mA signal.