Proportional Actuator (MASD) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
Proportional Actuator can be selected if the coil is controlled by a proportional valve that takes a 0–10 VDC or 4–20 mA signal.