Chilled Water (MASD) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The section is used to define the properties of a chilled water coil. This type of coil supports proportional, incremental, or two position control types, as well as several options.