Coils (Common Heating-Cooling) (MASD) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

These selections provide the logic to control a Common Heating-Cooling (also known as 2-pipe) coil.

Common Heating-Cooling cannot be selected if either Cooling or Reheat is selected.

The Remain in Control Shutdown Strategy is available only when a proportional valve is selected (with either proportional or incremental actuator).

The Loss of Airflow Strategy options are available only when the Automatic Restart option for the Supply Fan Status Loss of Airflow Strategy is selected.