Mixed Air Single Duct Applications - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The Mixed Air Single Duct application allows programming of many common Air Handling Unit configurations through the Tool. This application supports the following:
  • Supply fans and return or relief fans
  • Interlocked exhaust fans
  • Temperature control strategy
  • Economizer and minimum OA section options
  • Preheat, cooling, reheat, or dual temperature coils
  • Humidifier, dehumidifier, or both

See the following sections for information on this application’s logic and selections.See the Upgrading System Files section for a list and description of the module and System Selection changes that were made since the last release of the tool.