Occupancy Control (OASD) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

These selections provide the logic for Occupancy Mode Determination.

The selection options for Occupancy Control are:

  • Always Occupied

  • Scheduled Occupancy

    • Override Support

    • Occupancy Switch (BI)

    • Unoccupied Strategy

      • Intermittent Night Operation

      • Off during Unoccupied

If any options are selected for separate Occupied and Unoccupied Setpoints or Temporary Occupancy, the Always Occupied option cannot be selected.