Dehumidification Control (OASD) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

These selections provide the logic for dehumidification control.

The selection options for Dehumidification Control are:

  • Zone Humidity

  • Exhaust Air Humidity

Dehumidification cannot be selected unless both Cooling and Reheat are selected.