Monitored Safeties (OASD) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

These selections provide inputs for monitoring equipment safeties. The High and Low Static Pressure Switch inputs and High and Low Temperature Switch inputs are connected to the Emergency Mode Sequencer and shut down the application when tripped.

The selection options for Monitored Safeties are:

  • Discharge

    • High Static Pressure Switch

    • Smoke Detector

    • Low Static Pressure Switch
  • Exhaust

    • Low Static Pressure Switch

    • Smoke Detector

    • High Static Pressure Switch

  • Low Limit Temperature Switch

  • High Limit Temperature Switch

  • Humidity Alarm

  • Fire Dampers
    • (Options for One through Eight)
    • Fire Damper Alarm Reset Strategy
      • Automatic Restart

      • Manual Restart

        • Unit Reset Switch (BI)