Modules (OADD Monitored Safeties) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The Monitored Safeties selection loads the following modules in these Control View columns:

Inputs

  • DAPHI-A (Discharge Air High Duct Pressure)

  • DA-SD (Discharge Air Smoke Alarm)

  • EAPLO-A (Exhaust Air Low Duct Pressure)

  • EA-SD (Exhaust Air Smoke Alarm)

  • LT-A (Low Temperature Alarm)

  • HT-A (High Temperature Alarm)

  • HUMHI-A (Humidity High Limit)

See the Input Modules section.