Features and benefits - Metasys - LIT-1900386 - Software Application - Controller Configuration Tool - 16.0

Controller Configuration Tool (CCT) Catalog Page

Brand
Metasys
Product name
Controller Configuration Tool
Document type
Catalog Page
Document number
LIT-1900386
Version
16.0
Revision date
2023-09-06
Language
English
The following features are available at Release 15.0 and later:
  • Support for Displays—There is now a Default option available for displays on Release mode 10.6 or later, which means the password is determined by the device.
  • Support for Displays—Adds display firmware to SA Bus Firmware when completing a Transfer to Device or Download.
The following features are available at Release 14.0 and later:
  • Support for new Tier 4 Sensor/Actuator (SA) bus devices—You can add new Tier 4 SA Bus devices to CCT as package files. Use the Import option in the Define Hardware > Packages tab. When the Tier 4 SA Bus device is imported as a package file, you can add it as an SA Device in the Define Hardware > Controller Selection tab.
  • Update notifications—You can choose when you update your software with the new CCT update feature.
  • Support for BACnet Protocol Revision 18—A new MS/TP Controller Network Port object displays for supported devices in the Device Information folder in the Advanced tab.
The following feature is available at Release 13.1:
  • SNC Support—Provides you with the ability to commission and configure the applications of SNC devices.

The following features are available from Release 13.0 and later:
  • FSM Explorer—Provides a new way of viewing the Finite State Machine (FSM) in Configuration, Simulation and Commissioning mode.
  • New CAF Workflow—Helps you pick the correct Release Mode for your application.
  • Transfer to Device (Download) Enhancements—You can control when to activate transferred files on a controller and enable and disable the logic of applications in a device.
  • Support for SA Bus Provisioning—Provides the ability to update the firmware of all devices attached on the SA Bus. You can check the status of SA Bus devices in the Transfer Wizard.
  • BBMD Functionality—Provides you with the ability to configure IP controllers with BACnet Broadcast Management Device (BBMD) enabled.
  • N2 Application Transfer—Facilitates the transfer of N2 applications to N2 capable devices without requiring explicit communication switching.