CCT and Field Controller Package Licensing - Metasys - LIT-1900386 - Software Application - Controller Configuration Tool - 16.0

Controller Configuration Tool (CCT) Catalog Page

Brand
Metasys
Product name
Controller Configuration Tool
Document type
Catalog Page
Document number
LIT-1900386
Version
16.0
Revision date
2023-09-06
Language
English

CCT software and field controller package files require license activation. You can license CCT and field controller packages using the Software Manager, which is installed through the CCT installation wizard. For more information about software licensing, refer to the Software Manager Help (LIT-12012389).

Field controller package files are bundled separately. You can use the licensing infrastructure to download package files, and the Package Importer wizard to install them.

For more information about licensing and how to install field controller package files, refer to CCT Installation Instructions (LIT-12011529).