If a switch needs to be removed, label each Ethernet cable with the port to which it is connected before you disconnect it.
If a switch needs to be replaced, remember to remove the SD card. The SD cards contains all of the information needed to set up and configure a replacement switch.
If you need to replace a switch that is experiencing problems, note the switch serial number. You require this serial number to obtain support from Cisco’s SmartNet support program.