Cisco IOS reference - Metasys - LIT-12013055 - Gateway/Router - Cisco Switch - 12.0

Cisco IE 2000 and IE 4010 Ethernet Switches for Metasys Networks Installation Instructions and Troubleshooting Guide

Product
Network and Communications > Cisco Switches > Cisco Switch
Document number
LIT-12013055
Version
12.0
Revision date
2022-07-08

You do not need to use Cisco IOSĀ® commands to configure typical installations. You can use the IP Network Wizard instead. The following sections are included to support advanced configuration and troubleshooting. For detailed descriptions of Cisco IOS commands, refer to the Cisco IOS Configuration Fundamentals Command Reference, available at https://www.cisco.com/c/en/us/td/docs/ios/fundamentals/command/reference/cf_book.html

To access the command line interface of the switch, use a remote terminal session, such as SSH, from a laptop connected to the terminal point. Alternatively, the two console ports on the switch also give access to the command line, through a serial interface. The two console ports have different form factors: one is RJ-45 and other is USB (5-pin mini-Type B connector).

The command prompt indicates the command mode. Most commands are available from only one mode. There are many command modes, including the following.

Table 1. IOS command line prompt modes
Prompt Mode
> This is the least privileged mode, and has the smallest command set.
# This is the privileged mode, from which one can change the switch configuration.

The flavors of privileged mode include the following.

Table 2. IOS Command Line prompt modes in privileged mode
Prompt Tasks completed in this mode
(config)# Editing a switch configuration.
(dhcp-config)# Editing the DHCP configuration of switch.
(config-if)# Editing the configuration of a switch interface.

The switch ports are physical interfaces. Other interfaces, like switch virtual interfaces (SVIs), are logical interfaces. You configure logical interfaces at the same time that you create them.

When typing commands, it is helpful to know the following:

  • Use the up arrow to retrieve previous commands.
  • Use the tab key for command completion. There are abbreviated versions of most commands.
  • Use a ? to get help on options that could be typed at this point. For example, to view help on the show command, enter show ?.
  • Use the tab key to auto-complete. For example, typing sh+TAB+SPACE+run+TAB fills the command line with show running-config.