Configuring integrated feedback using the System Selection Wizard - Metasys - LIT-12013631 - M4-CVM Actuator - Release 11.0

CV Series Controller Actuator Feedback Application Note

Brand
Metasys
Product name
M4-CVM Actuator
Document type
Application Note
Document number
LIT-12013631
Version
Release 11.0
Revision date
2022-01-26
Product status
Active
Language
English

About this task

To configure integrated feedback using the System Selection Wizard, complete the following steps:

Procedure

  1. Open CCT.
  2. From the File menu, click New.
  3. In the New System window, type a name for your system in the System Name text box.
  4. From the System Type list, select VAV.
  5. From the System Configuration list, choose Single Duct and click OK.
  6. In the System Selection Wizard window, under Supply Duct Actuator > Integrated Actuator, tick the Integrated Feedback check box.
  7. Complete the options for your new system and click Finish. The application builds and appears in the Tool.
    Note: After the application builds, two new network inputs appear under the DPR-POS sensor. The first, DPR-POS-PRESENT, is a Boolean value that when True indicates that integrated actuator feedback is onboard. The second, DPR-POS-AUTOCAL-EN, is a Boolean value that when True indicates that the input range low and input range high attributes of the DPR-POS sensor AI are determined automatically by the integrated feedback based on the end stops of actuator rotation.
  8. In the upper-right of the Application pane, choose Define Hardware.
  9. On the Controller Selection tab, locate and select the CVM03050 or CVE03050 device package.
  10. Complete the selections for controller setup and click Finish.