Add two new network inputs, and connect each input to one of the control points previously added.
About this task
To add new network inputs, complete the following steps:
Procedure
- In the upper right corner of the Network Inputs dialog box, click the Add icon. The New Module Selection dialog box appears.
-
Click the Count field in the row for INPUT-BOOLEAN and change the count to 2.
Figure 1. New module selection dialog box
- Click Finish to return to the Network Inputs dialog box.
- Right-click INPUT-BOOLEAN-1.
- Click Rename. Rename the input as DPR-POS-AUTOCAL-EN to match the name of the corresponding miscellaneous control point.
- Right-click INPUT-BOOLEAN-2.
- Click Rename. Rename the input as DPR-POS-PRESENT to match the name of the corresponding miscellaneous control point.
-
Right-click DPR-POS-AUTOCAL-EN input and select
View Details.
Figure 2. Network inputs: view details
- Click Edit on the upper left corner of the details view window.
- Set the Default Value attribute to True.
- Click Apply on the upper left corner and then click Close to return to the Network Inputs dialog box.
- Right-click the DPR-POS-PRESENT input.
-
Repeat steps 10 and 12.
Note: Set the BACnet Exposed attribute to False.
- Select the DPR-POS-AUTOCAL-EN input, then select the Connections tab.
-
Right-click the DPR-POS-AUTOCAL-EN in the Output
column and select Make Connection.
Figure 3. Make connection view
- Select DPR-POS-AUTOCAL-EN under Hardware>Outputs and click OK.
- Repeat steps 14-16 for the DPR-POS-PRESET input.