Configuring integrated feedback manually for dual-duct VAV systems - Metasys - LIT-12013631 - M4-CVM Actuator - Release 11.0

CV Series Controller Actuator Feedback Application Note

Product
Valves and Actuators > Actuators > M4-CVM Actuator
Document type
Application Note
Document number
LIT-12013631
Version
Release 11.0
Revision date
2022-01-26
Product status
Active

For dual-duct VAV systems, you can add the integrated feedback analog input manually by selecting it from the palette. For further information, refer to the Adding Modules section of the Controller Tool Help (LIT-12011147).

About this task

To configure the integrated feedback manually, complete the following steps:

Procedure

  1. In the upper-right of the Inputs dialog box, click the Add icon.
  2. Type Supply Damper in the Filter field. Locate the Supply Damper application with the signal type, Integrated Feedback.
    Figure 1. Supply damper module with integrated feedback signal

  3. Click the Count field and change the count to 1.
  4. Click Finish.