Add two new network inputs, and connect each input to one of the control points previously added. The following example is based on the cold deck damper being controlled by the CVM/CVE with integrated position feedback.
About this task
To add new network inputs, complete the following steps: