Adding miscellaneous control points for dual-duct VAV systems - Metasys - LIT-12013631 - M4-CVM Actuator - Release 11.0

CV Series Controller Actuator Feedback Application Note

Product
Valves and Actuators > Actuators > M4-CVM Actuator
Document type
Application Note
Document number
LIT-12013631
Version
Release 11.0
Revision date
2022-01-26
Product status
Active

Miscellaneous control points enable the hardware to detect if integrated feedback is present in order to determine if automatic calibration of the feedback position is enabled.

About this task

To add miscellaneous control points, complete the following steps:

Procedure

  1. In the upper right of the Output Miscellaneous window, click the Add icon.
  2. Complete one of the following options:
    1. If the integrated actuator on the CVM/CVE controls the hot deck, complete the following steps:
      1. Type Hot Deck in the Filter field. Locate the Autocalibration Flag and the Integrated Position Flag function.
      2. Click the Count box and change the count to 1 for both functions.
      3. Click Finish.
    2. If the integrated actuator on the CVM/CVE controls the cold deck, complete the following steps:
      1. Type Cold Deck in the Filter field. Locate the Autocalibration Flag and the Integrated Position Flag function.
      2. Click the Count box and change the count to 1 for both functions.
      3. Click Finish.