Configuring dual-duct VAV systems - Metasys - LIT-12013631 - M4-CVM Actuator - Release 11.0

CV Series Controller Actuator Feedback Application Note

Brand
Metasys
Product name
M4-CVM Actuator
Document type
Application Note
Document number
LIT-12013631
Version
Release 11.0
Revision date
2022-01-26
Product status
Active
Language
English
Configure the controller with Controller Configuration Tool (CCT) version 14.0 or later, using Release Mode 10.5, Firmware 9.0 to maximize hardware capability. For further information, refer to the Controller Tool Help (LIT-12011147).
Note: You cannot configure an application from the system selection tree with integrated actuator feedback for dual-duct VAV systems. You can only manually configure integrated actuator feedback for dual-duct VAV systems.