Calibration position - Metasys - LIT-12013631 - M4-CVM Actuator - Release 11.0

CV Series Controller Actuator Feedback Application Note

Brand
Metasys
Product name
M4-CVM Actuator
Document type
Application Note
Document number
LIT-12013631
Version
Release 11.0
Revision date
2022-01-26
Product status
Active
Language
English

The voltage feedback signal that corresponds to the 100% open position is learned each time 0% or 100% is reached.

To turn off the auto-calibration of the voltage feedback signal, select the parameter name in the output section and set its value to FALSE. Set values in units of volts for the Input Range High and Input Range Low attributes that correspond to 100% open and 0% open, respectively.