This fault occurs when the actuator stroke time of travel is greater than the value entered for the effective stroke time.
About this task
Note: You can add
this alarm if the parent network engine is at Release 11.0 or later.
Note: Configure the
Effective Stroke Time parameter during the commissioning phase.
To detect
that the field stroke time is greater than the user-entered value, complete the
following steps: