Completing an offline deactivation in the License Portal - Johnson Controls - Metasys - LIT-12012392 - Software Application - Software Licensing - 3.0

Branch License Manager License Portal Help

Product
Building Automation Systems > Authentication and Licensing > Software Licensing
Document type
User Guide
Document number
LIT-12012392
Version
3.0
Revision date
2020-10-30

About this task

Note: These steps must be completed or the license cannot be used on another machine.

After you use the license deactivation file in the Software Manager and retrieve the license release file, follow these steps to complete the offline deactivation process in the License Portal:

Procedure

  1. In the License Portal, click Next in the Offline Deactivation wizard.
  2. Click Choose Files to browse and select the file, or drag and drop the license release file to the Drag & drop your files here area in the Offline Deactivation wizard.
  3. Click Next. The following message appears to indicate a successful deactivation: Deactivation successful.
  4. Click Close to finish.