Term | Description |
---|---|
ABCS |
Authorized Building Control Specialist. Johnson Controls contracts ABCSs to sell and distribute certain Johnson Controls products. |
Activated license |
A license activated using either the online or offline activation process with the Software Manager. |
Activation |
A user action to initiate the activation of a software entitlement. The result is a licensed feature. |
AOMS |
Advanced Order Management System. Sales, branches and ABCSs use the AOMS to purchase or order products. It also provides a customer interface for branches and ABCSs. |
Available license |
A license available for activation using either the online or offline activation process with the Software Manager. |
Branch License Manager (BLM) |
A Branch License Manager (BLM) manages requests for technician software licenses for their designated branch. |
Deactivate |
A user action to initiate the deactivation of an activated license. If you do not activate another license for the feature, the result is an unlicensed feature. When you deactivate a license, you can activate this license on another machine. |
Entitlement |
Refers to a user's right to use one or more software features. |
Expired |
Refers to the license status of a software feature when its license passes its expiration date. |
Feature |
An aspect of software identified by name and version as something that can be independently licensed. |
Grace priod |
Refers to the period of time provided for an emergency grace license. A user starts a grace period through the Software Manager. You cannot pause or stop a grace period when started. |
License |
A license defines the terms of use for the associated software feature and version combination. |
License activation file |
A file provided to a user by the online License Portal as part of the offline activation process. The Software Manager processes the content of the file to complete the offline activation process for a software feature. |
Licensed |
Refers to the license status of a software feature with an activated and unexpired license. |
License deactivation file |
A file provided to a user by the online License Portal as part of the offline deactivation process. The Software Manager processes the content of the file to revoke the license on the offline machine and to generate a license release file. |
License portal |
The online License Portal provides a user interface for authorized users to access software product licensing information, and actions and links for downloading software and documentation. The License Portal's available features and actions depend on the role of the logged-in user. |
License release file |
A file created by the Software Manager as part of the offline deactivation process. The user must upload the license release file to the License Portal to complete the offline deactivation process and release the license for activation again. |
License status |
Indicates if a software feature is currently licensed. |
Machine |
Any device on which licensable software may exist. |
Machine tag |
A user-friendly label associated with a specific machine based on its given system ID. Machine tags make it easier for a user to determine what software is licensed on a particular machine. |
Offline activation |
A manual process used to activate a license on a machine that has no Internet connection, or is the customer's preferred activation method. Offline activation requires both the Software Manager and access to the online License Portal from a machine connected to the Internet. |
Offline deactivation |
A manual process used to deactivate a license on a machine that has no Internet connection, or it is the customer's preferred deactivation method. Offline deactivation requires both the Software Manager and access to the online License Portal from a machine connected to the Internet. |
Online activation |
An automated process used to activate a license using the Software Manager on a machine that has an Internet connection. |
Online deactivation |
An automated process used to deactivate a license using the Software Manager on a machine that has an Internet connection. |
Product code | A unique code assigned to a product so it can be identified. |
Product key |
A code used to activate a feature for an entitlement. The entitlement system generates the product key used to activate the feature license. |
Salesforce |
Salesforce is a Customer Relationship Management (CRM) platform to provide Johnson Controls Sales employees with the ability to request sales trials and sales demos. |
Software Manager |
Provides a user interface for users to view and manage licenses for software. |
Start grace period |
An action a user takes to initiate the start of an emergency Grace license for a software feature. |
Super BLM |
A Super BLM can manage requests for technician software licenses for all branches. |
System ID |
A code that uniquely identifies a physical or virtual machine. The local license service on a machine determines the system ID and displays it on the Software Manager's main screen. Refer to Software Manager Help (LIT-12012389). |
Unlicensed |
Refers to the license status of a software feature that has no active and valid licenses. |