Overview - Metasys - LIT-12013511 - Bert plug integration - Bert Plug Load Control - 10.1

Bert Plug Load Control and Metasys Integration Guide

Product
Integrations > Bert Plug Integrations > Bert Plug Load Control
Document number
LIT-12013511
Version
10.1
Revision date
2020-02-21

This document describes the Bert® plug load monitoring and control system of devices that can be easily integrated with any release of the Metasys® Building Automation System (BAS) supporting a BACnet IP integration.

Bert devices are smart plugs and inline circuit controllers that can monitor and control the electrical plug loads for individual devices or circuits in a building. For installation flexibility, there are three types of Bert devices.

Figure 1. Bert Inline I Series (120/240/277V)

The Bert Inline I Series (120/240/277V) has the following characteristics:

  • 20A measurement and control for circuits and hardwired devices
  • Series or parallel wiring
  • Flexible, low-cost sub-metering solution
  • Automatic receptacle control for ASHRAE 90.1 and CA Title 24 code compliance
  • Manual override button allows you to turn devices on during off-peak hours
  • 802.11 WiFi network communication on 2.4 or 5 GHz
  • LED indicator for on/off and network status

See https://Bertbrain.com/hardware-inline-series-Bert-120-i/ for further information.

Figure 2. Bert Inline IR Series (120/240V)

The Bert Inline IR Series (120/240V) has the following characteristics:

  • 20A measurement and control for circuits and hardwired devices
  • Series or parallel wiring
  • Split-wiring option for individual receptacle control
  • Flexible, low-cost sub-metering solution
  • Automatic receptacle control for ASHRAE 90.1 and CA Title 24 code compliance
  • Manual override button enables users turn devices on during off hours
  • 802.11 WiFi network communication on 2.4 or 5 GHz
  • LED indicator for device power and network status

See https://Bertbrain.com/hardware-inline-series-Bert-120-ir/ for further information.

Figure 3. Bert Smart Plug

The Bert Smart Plug has the following characteristics:

  • Enhanced network security: WPA/WPA2-Enterprise with radius server authentication
  • Improved network performance: 802.11 n, 2.4 or 5 GHz
  • Easy plug-in installation
  • Optional tamper-proof screw
  • Manual override button enables users turn devices on during off hours
  • LED indicator for on/off and network status

See https://Bertbrain.com/hardware-Bert-smart-plug-series-110-x/for further information.