Integration with Metasys UI - Metasys - LIT-12013511 - Bert plug integration - Bert Plug Load Control - 10.1

Bert Plug Load Control and Metasys Integration Guide

Product
Integrations > Bert Plug Integrations > Bert Plug Load Control
Document number
LIT-12013511
Version
10.1
Revision date
2020-02-21

Use the Metasys UI to manage Bert device information, monitor energy usage, and view equipment summaries. For information on using the Metasys UI, refer to the Metasys UI Help (LIT-12011953).

Figure 1. An example of the Bert device information page in Metasys UI ???