You can download a Bert controller template from the Global Library site: https://globallibrary.azurewebsites.net/#/controllertemplate. The controller template defines a set of points that are available in a Bert device. The controller template is required if you use the Rapid Archive to complete the integration process. For more information, refer to the Controller Templates section in the Metasys SCT Help (LIT-12011964).
Figure 1. Bert Controller Template in SCT
To import the controller template into an SCT archive, complete the following steps:
- Download the controller template file from Johnson Controls or create one in SCT.
- Launch the SCT, and then open an archive.
- In the All Items tree, expand the Configuration Data folder.
- Right-click the SCT Controller Templates folder, and then click Import Template.
- Navigate to the location of the controller template you downloaded, select the template, then click Import.
- After the import is complete, a confirmation message appears. Click OK. The controller template imports and is listed under the SCT Controller Templates folder.