Linking a controller template to an equipment definition in SCT - Metasys - LIT-12013511 - Bert plug integration - Bert Plug Load Control - 10.1

Bert Plug Load Control and Metasys Integration Guide

Product
Integrations > Bert Plug Integrations > Bert Plug Load Control
Document number
LIT-12013511
Version
10.1
Revision date
2020-02-21

After you import both the equipment definition and the controller template, you must create a link between them.

  1. Open the controller template in a focus window and select the Configuration tab.
  2. Click Edit.
  3. In the Definition Link parameter, click the browse icon to open the Select Item wizard.
  4. Navigate to the equipment definition and select it.
  5. Click OK.
  6. Click Save.