Consolidating spaces - Metasys - LIT-12013511 - Bert plug integration - Bert Plug Load Control - 10.1

Bert Plug Load Control and Metasys Integration Guide

Product
Integrations > Bert Plug Integrations > Bert Plug Load Control
Document type
Integration Guide
Document number
LIT-12013511
Version
10.1
Revision date
21/02/2020
To import the Rapid Archive Schedule into the Rapid Archive Field Controller wizard, you must include information in the Site/Building/Floor and Leaf Space columns. For example, if a Bert device is located at BE Headquarters/Campus 507/Building 1/Floor 3/Room 201, in the Site/Building/Floor column enter BE Headquarters/Campus 507/Building 1/Floor 3, and in the Leaf Space column, enter Room 201.
Note: Before you enter space information, you may need to consolidate multiple different space hierarchies. For example, the spaces for Bert devices may be different than the spaces for HVAC zones or lighting zones. It is important to use a single space hierarchy for all integrated building systems. If you do not consolidate to a single space hierarchy, then you may unintentionally create duplicate definitions for spaces in the Metasys UI, and navigating the building can be cumbersome.