Completing the Bert device schedule in Excel - Metasys - LIT-12013511 - Bert plug integration - Bert Plug Load Control - 10.1

Bert Plug Load Control and Metasys Integration Guide

Product
Integrations > Bert Plug Integrations > Bert Plug Load Control
Document number
LIT-12013511
Version
10.1
Revision date
2020-02-21

Once you export the Bert device information from the Bert Connect Gateway, you can copy the names and BACnet instance numbers into an official RAC schedule spreadsheet where you can continue to add more data, including space names, equipment names and references, NAE information, and the equipment definition and controller template names.

For detailed information on use of the Rapid Archive Schedule, refer to the Rapid Archive Schedule Population in the Rapid Archive Wizard section in the Metasys SCT: System Configuration Tool Help (LIT-12011964).