Metasys NAE - Metasys - LIT-12013511 - Bert plug integration - Bert Plug Load Control - 10.1

Bert Plug Load Control and Metasys Integration Guide

Product
Integrations > Bert Plug Integrations > Bert Plug Load Control
Document number
LIT-12013511
Version
10.1
Revision date
2020-02-21

An NAE is a web-enabled, IP-based, supervisory engine that connects BAS networks to IP networks. An NAE can operate as a stand-alone site director or can be part of a larger network reporting to a Metasys server. You install the Johnson Controls® Launcher application on a computer to access the NAE, and then monitor and control BAS devices and systems using the NAE or Metasys server user interfaces from a computer or mobile device. Refer to Launcher Help (LIT-12011742) for further information.

Figure 1. NAE