Inserting field points - Metasys - LIT-12013511 - Bert plug integration - Bert Plug Load Control - 10.1

Bert Plug Load Control and Metasys Integration Guide

Product
Integrations > Bert Plug Integrations > Bert Plug Load Control
Document number
LIT-12013511
Version
10.1
Revision date
2020-02-21

If you are continuing from the Field Device Extension wizard above, proceed to Step 3 with Select Definition Mode.

  1. Drag the Bert device object from the navigation panel to the display panel. The Focus tab for the device appears.
  2. Click Insert Field Point. The Insert Point wizard appears.
  3. In the Destination window, select the Bert device if not already selected and click Next.
  4. In the Select Definition Mode window, click Invoke Auto Discovery to begin a BACnet point discovery.
  5. The Auto Detect Utility wizard appears. This wizard shows that a discovery is in progress. When the new points are discovered from the device, they appear in the discovery results list. Click Close when the discovery is complete. The Point Mapping wizard appears.
  6. Use the Point Mapping dialog to select the points you want to map.