Installation procedures - Metasys - LIT-12013511 - Bert plug integration - Bert Plug Load Control - 10.1

Bert Plug Load Control and Metasys Integration Guide

Product
Integrations > Bert Plug Integrations > Bert Plug Load Control
Document type
Integration Guide
Document number
LIT-12013511
Version
10.1
Revision date
21/02/2020
Follow these best practice guidelines when installing Bert devices:
  • Record the MAC address of each Bert device and the location it was installed. This is required for the commissioning process.
  • When power is applied to the circuit, perform a quick electrical test to ensure that power is being delivered to the downstream outlet or circuit. If no power is delivered downstream of the Bert device, and the wiring installation appears to be correct, the Bert device may be in the OFF state.
  • To change the state of the Bert device, hold the small button on the Bert device (that should be flashing a green LED) for 4 seconds. You hear a click to indicate the relay has turned ON. You can then re-test the downstream outlet or circuit for power.