Installing Bert devices - Metasys - LIT-12013511 - Bert plug integration - Bert Plug Load Control - 10.1

Bert Plug Load Control and Metasys Integration Guide

Product
Integrations > Bert Plug Integrations > Bert Plug Load Control
Document number
LIT-12013511
Version
10.1
Revision date
2020-02-21

A licensed electrician must install each of the inline Bert devices. To install the Bert devices, the electrician must follow the wiring diagram and instructions. For further information, refer to https://bertbrain.com.