Adding a new supervisory device to a BACnet/SC site - Metasys - LIT-12013959 - 13.0

BACnet/SC Workflow Technical Bulletin

Brand
Metasys
Document type
Technical Bulletin
Document number
LIT-12013959
Version
13.0
Revision date
2023-09-29
Product status
Active
Language
English

About this task

Modifying a supervisory device to connect to a Site Director does not involve BACnet/SC, so the workflow for this is identical to adding a supervisory device to a BACnet/IP site. After you add the supervisory device to the Site Director, follow the steps in Enabling BACnet/SC for IP equipment controllers or supervisory devices.

Important: If the supervisory device is already communicating with its equipment controllers by using Secure Connect Only Mode, you must first set it and all its devices back to Ethernet IP Only Mode and then connect to the new site. If the certificates have a different CA, then you must replace the certificates or add the new CA to the site, so that the site devices will trust the new certificates.