BACnet/SC use cases - Metasys - LIT-12013959 - 13.0

BACnet/SC Workflow Technical Bulletin

Brand
Metasys
Document type
Technical Bulletin
Document number
LIT-12013959
Version
13.0
Revision date
2023-09-29
Product status
Active
Language
English

The following use cases cover a user enabling BACnet/SC on devices on a site that was upgraded to support BACnet/SC. The solution does not support enabling BACnet/SC in the archive as part of the upgrade, because devices cannot communicate through BACnet/SC until they have trusted certificates signed by the CA.