Acquiring a CA for the site - Metasys - LIT-12013959 - 13.0

BACnet/SC Workflow Technical Bulletin

Brand
Metasys
Document type
Technical Bulletin
Document number
LIT-12013959
Version
13.0
Revision date
2023-09-29
Product status
Active
Language
English
A CA is an entity that issues the operational certificates to use for communication on a site. You must decide what will be the certificate authority used to generate the operational certificates. You can instruct the customer's IT department to act as the CA. Submit a request to the customer by completing a Request for Information (RFI), or by sending an email to the customer.
Note: A third-party vendor of BACnet/SC devices could also act as the CA.