Adding an Averaging Extension - Metasys - LIT-1201531 - System Integration - BACnet Controller Integration - 11.0

BACnet Controller Integration Technical Bulletin

Product
Controls > BACnet Controls > BACnet Controller Integration
Document type
Technical Bulletin
Document number
LIT-1201531
Version
11.0
Revision date
2022-02-09

About this task

Procedure

  1. In the Extensions Wizard, click New in the Averaging row. The Insert Averaging Wizard Select Attribute screen appears.
    Figure 1. Insert Averaging Wizard (Select Attribute Screen)

  2. Select an object in the top of the screen and an attribute in the bottom of the screen and click Next.
    Note: Click other to display a list of available attributes.
  3. Follow the prompts in the Wizard to complete the addition of an Averaging Extension.
  4. Click Finish. The Extensions Wizard appears with the new attribute listed under Averaging.