Adding an Alarm Extension - Metasys - LIT-1201531 - System Integration - BACnet Controller Integration - 11.0

BACnet Controller Integration Technical Bulletin

Product
Controls > BACnet Controls > BACnet Controller Integration
Document type
Technical Bulletin
Document number
LIT-1201531
Version
11.0
Revision date
2022-02-09

About this task

Note: To add a BACnet intrinsic alarm, refer to the M-Series Workstation Interface to the NAE Application Note (LIT-1201655).

Procedure

  1. In the Extensions Wizard, click New in the Alarm row. The Insert Alarm Wizard Select Attribute screen appears.
    Figure 1. Insert Alarm Wizard (Select Attribute Screen)

  2. Next.
    Note: Click other to display a list of available attributes. Select an object in the top of the screen and an attribute in the bottom of the screen and click
  3. Follow the prompts in the Wizard to complete the addition of an Alarm Extension.
  4. Click FinishSelect an object in the top of the screen and an attribute in the bottom of the. The Extensions Wizard appears with the new attribute listed under the Alarm tab.