Adding a Totalization Extension - Metasys - LIT-1201531 - System Integration - BACnet Controller Integration - 11.0

BACnet Controller Integration Technical Bulletin

Product
Controls > BACnet Controls > BACnet Controller Integration
Document number
LIT-1201531
Version
11.0
Revision date
2022-02-09

About this task

Procedure

  1. In the Extensions Wizard, click New in the Totalization row. The Insert Totalization Wizard Select Attribute screen appears.
    Figure 1. Insert Totalization Wizard (Select Attribute Screen)

  2. Select an object in the top of the screen and an attribute in the bottom and click Next.
    Note: Click other to display a list of available attributes.
  3. Select Totalization type from the available options on the right (if available).
  4. Follow the prompts in the Wizard to complete the addition of a Totalization Extension.
  5. Click Finish. The Extensions Wizard appears with the new attribute listed under the Totalization tab.