Using the Relearn feature - Metasys - LIT-1201531 - System Integration - BACnet Controller Integration - 11.0

BACnet Controller Integration Technical Bulletin

Product
Controls > BACnet Controls > BACnet Controller Integration
Document number
LIT-1201531
Version
11.0
Revision date
2022-02-09

About this task

The Relearn feature uses Auto Discovery and requires that the supervisory controller be online with the BACnet network to discover Field Devices and Field Points.

Procedure

  1. Select the BACnet Integration object from the Navigation tree.
  2. Click the Engineering tab and click the Relearn button that appears below the tab.
  3. Discovery begins automatically and finds all new BACnet devices on the network. After Discovery, the new devices appear in the Integration Tree and in the Integration View.
  4. When Discovery is complete, close the Auto Discovery box.