Connecting to BACnet devices - Metasys - LIT-1201531 - System Integration - BACnet Controller Integration - 11.0

BACnet Controller Integration Technical Bulletin

Product
Controls > BACnet Controls > BACnet Controller Integration
Document type
Technical Bulletin
Document number
LIT-1201531
Version
11.0
Revision date
2022-02-09

To connect and integrate BACnet devices into the Metasys system, connect the BACnet devices to the same IP network as the supervisory controller used for the BACnet system integration.

The devices must have the same BACnet Network Address and BACnet/IP Port number (UDP port) as assigned to the supervisory controller to which the device is to be integrated. These values can be seen in the NAE Focus tab.