In its default configuration, third-party BACnet/IP devices can
only see the integrated BACnet objects of the network engine. If the BACnet Routing mode
is set to Enabled in the network engine, then other BACnet devices on the IP network are
able to communicate directly with BACnet MS/TP devices. See Enabling the routing mode.
Note: In most cases, enabling routing
is not recommended.