BACnet Controller Integration overview - Metasys - LIT-1201531 - System Integration - BACnet Controller Integration - 11.0

BACnet Controller Integration Technical Bulletin

Product
Controls > BACnet Controls > BACnet Controller Integration
Document type
Technical Bulletin
Document number
LIT-1201531
Version
11.0
Revision date
2022-02-09

As a BACnet integrator, the supervisory controller monitors and supervises a network of BACnet devices and acts as a BACnet operator workstation for all integrated controllers. Data is presented to the operator through the Site Management Portal UI of the supervisory controller. Other BACnet devices on the network can read from and write to the BACnet objects within the supervisory controller.