Deleting extensions from an object - Metasys - LIT-1201531 - System Integration - BACnet Controller Integration - 10.1

BACnet Controller Integration Technical Bulletin

Product
Controls > BACnet Controls > BACnet Controller Integration
Document number
LIT-1201531
Version
10.1
Revision date
2021-10-08

About this task

Procedure

  1. Select a field device or a field point that contains the extensions to delete.
  2. On the Action menu, select Show Extensions. The Extension Wizard starts.
  3. Select the check boxes next to the extensions you want to delete.
  4. Click Delete for each extension.

    Clicking Delete in any extension row deletes only the checked extensions in that row. For example, in the Extension Wizard, click both Resource Delete and Alarm Delete to delete both checked extensions.

  5. Click Done when finished.