Copying extensions to a Field Device or Field Point (offline only) - Metasys - LIT-1201531 - System Integration - BACnet Controller Integration - 10.1

BACnet Controller Integration Technical Bulletin

Brand
Metasys
Product name
BACnet Controller Integration
Document type
Technical Bulletin
Document number
LIT-1201531
Version
10.1
Revision date
2021-10-08
Language
English

About this task

Procedure

  1. Select a field device or a field point that contains the extensions to copy.
  2. On the Action menu, click Show Extensions. The Extension Wizard starts.
  3. Select the check boxes for the extensions that you want to copy and click Copy Checked Extensions at the bottom of the Wizard.
  4. Click Done.
  5. In the Navigation Tree, select the desired field device or field point destination.
  6. On the Edit menu, click Paste. This adds the copied extensions to the selected field device or field point.
  7. Drag the field device or field point to the Display frame (on the right) to verify that the new extensions are correct.