Adding a Load Extension - Metasys - LIT-1201531 - System Integration - BACnet Controller Integration - 10.1

BACnet Controller Integration Technical Bulletin

Brand
Metasys
Product name
BACnet Controller Integration
Document type
Technical Bulletin
Document number
LIT-1201531
Version
10.1
Revision date
2021-10-08
Language
English

About this task

Procedure

  1. In the Extensions Wizard, click New in the Load row. The Insert Load Wizard Select Attribute screen appears.
  2. Select an object in the top of the screen and an attribute in the bottom of the screen and click Next.
    Note: Click other to display a list of available attributes.
  3. Follow the prompts in the Wizard to complete the addition of a Load Extension.
  4. Click Finish. The Extensions Wizard appears with the new attribute listed under Load.